Note: These commands are accessible only for PNA-X models.
These Visual Basic and C# examples exercise various commands on the:
IFPathConfiguration Setup example
|
' Create / Get the PNA application Dim app Set app = CreateObject("AgilentPNA835x.Application") ' Preset the instrument app.Preset ' Get a channel interface on which to operate Dim chan Set chan = app.ActiveChannel ' Modify the Default configuration, and save it as “My Config” chan.PathConfiguration = "Default" ' Set the “Combiner” element to value “Reversed” chan.PathConfiguration.Element("Combiner").Value = "Reversed" ' Set the “Src1” element to value “High Power” chan.PathConfiguration.Element("Src1").Value = "High Power" ' Change the description text chan.PathConfiguration.DescriptionText = "Connect J8 to J9." ' Store the modified configuration chan.PathConfiguration.Store ("My Config") ' Set the instrument’s path config back to the default (req. 8) chan.PathConfiguration = "Default" ' Load a previously saved configuration onto channel 1 app.PathConfigurationManager.Load 1, "My Config" |
|
Type pnaType = Type.GetTypeFromProgID("AgilentPNA835x.Application", "PNA-NAME-HERE"); AgilentPNA835x.Application pna = (AgilentPNA835x.Application)Activator.CreateInstance(pnaType); AgilentPNA835x.Channel chan = (AgilentPNA835x.Channel)pna.ActiveChannel; // Preset the Instrument pna.Preset(); // Modify the Default configuration, and save it as "My Config" chan.set_PathConfiguration("Default"); // Set the "Combiner" element to value "Reversed" chan.get_PathConfiguration().get_Element("Combiner").Value = "Reversed"; // Change the description text chan.get_PathConfiguration().DescriptionText = "Connect J8 to J9."; // Store the modified configuration chan.get_PathConfiguration().Store("My Config"); // Set the instrument’s path config back to the default (req. 8) chan.set_PathConfiguration("Default"); // Load a previously saved configuration onto channel 2 pna.PathConfigurationManager.LoadConfiguration(1, "My Config"); |