Write-only
About Windows

ActivateWindow Method


Description

Makes a window object the Active Window.

In order to change properties on any of the active objects, you must first have a "handle" to the active object using the Set command. For more information, See Programming the Analyzer Object Model.

You do not have to make an object "Active" to set or read its properties remotely. But an object must be "Active" to change its values from the front panel.

 VB Syntax

app.ActivateWindow n

Variable

(Type) - Description

app

An Application (object)

n

(long) Number of the window to make active

Return Type

Window Object

Default

Not Applicable

Examples

app.ActivateWindow 4

C++ Syntax

HRESULT ActivateWindow(long WindowNumber)

Interface

IApplication

See the PNA Object Model