Write-only
About Markers

ActivateMarker Method


Description

Makes a marker the Active Marker. Use meas.ActiveMarker to read the number of the active marker.

 VB Syntax

meas.ActivateMarker(Mnum)

Variable

(Type) - Description

meas

A Measurement (object)

Mnum

(long integer) - the number of the marker to make active. Choose any marker number from 1 to 15.

Return Type

None

Default

Not Applicable

Examples

meas.ActivateMarker(1)'Write

C++ Syntax

HRESULT ActivateMarker(long lMarkerNumber)

Interface

IMeasurement

Remarks

Use ReferenceMarkerState to control the Reference marker.