Write-only
About Channels

Add (channels) Method


Description

Creates a channel and returns a handle to it. If the channel already exists, it returns the handle to the existing channel.

VB Syntax

chans.Add (item)

Variable

(Type) - Description

chans

A Channel collection (object)

item

(variant) - Channel number.

Return Type

Channel

Default

Not Applicable

Examples

chans.Add 3 'Creates channel 3

C++ Syntax

HRESULT Add(VARIANT numVal, IChannel** pChannel)

Interface

IChannels