Description |
Applies the mixer setup and turns the channel ON. (Performs the same function as the Apply button on the mixer setup dialog box.) Learn about the Scratch and Applied mixer properties |
VB Syntax |
obj.Apply |
Variable |
(Type) - Description |
|
obj |
A Mixer Interface pointer to the Measurement (object) Or |
Return Type |
Not Applicable |
Default |
Not Applicable |
Examples |
mxr.Apply |
C++ Syntax |
HRESULT Apply() |
Interface |
IMixer3 IConverter |
Last Modified:
|
2-Feb-2009 |
Added converter object |