Write-Read
Learn about the Pulsed Application

ConfigEnhancedNBIFAtten Method


Description

Sets PNA-X receivers to auto gain setting.

 VB Syntax

Pulsed.ConfigEnhancedNBIFAtten (PRF, RxWidth, IFAtten)

Variable

(Type) - Description

Pulsed

(interface)  An interface to the agilentpnapulsed.dll application interface.

PRF

(Double)  

[in] The Pulse Repetition Frequency.

RxWidth

(Double)

[in] Receiver gate width.

IFAtten

(Long Integer)

[out] IF attenuation value.

Return Type

Not Applicable

Default

Not Applicable

Example

See an example using this command.

C++ Syntax

HRESULT ConfigEnhancedNBIFAtten(double *pPRF, double *pWidth, long *pIF)

Interface

AgilentPNAPulsed.Application