Write-Read |
Learn about the Pulsed Application |
Description |
Note: This command is replaced by ConfigEnhancedNB2 Method This subroutine determines, then returns, the proper configuration for pulsed measurements on the PNA-X ONLY using the spectral nulling technique. The configuration returned needs to be sent to the PNA and any other related external equipment. The routine will take a desired Pulse Repetition Frequency (PRF) and measurement IFBW and return a possibly modified PRF and IFBW for proper pulsed operation on the PNA. |
VB Syntax |
Pulsed.ConfigEnhancedNB (PRF, BW, PhysicalIF, NCO, Stage1TapArray, Stage2TapArray, Stage3TapArray, FixedPRF) |
Variable |
(Type) - Description |
|
Pulsed |
(interface) An interface to the agilentpnapulsed.dll application interface. |
|
PRF |
(Double) The Pulse Repetition Frequency. [out] The pulse repetition frequency that has been optimized for use with the PNA. NOTE: This value may be different from the value requested. [in] The desired pulse repetition frequency. |
|
BW |
(Long) The PNA IF Bandwidth. [out] The PNA IF bandwidth that has been optimized for use with the PNA. NOTE: This value may be different from the value requested. Zero (0) is returned if no solution is found for the specified PRF and BW. [in] The desired PNA IF bandwidth. |
|
PhysicalIF |
(Double) Returns physical intermediate frequency. |
|
NCO |
(Double) Returns numeric controlled oscillator frequency. |
|
Stage1TapArray |
(Long array) Returns the stage 1 filter coefficients |
|
Stage2TapArray |
(Long array) Returns the stage 2 filter coefficients |
|
Stage3TapArray |
(Long array) Returns the stage 3 filter coefficients |
|
FixedPRF |
(Boolean) 1 (True) Signals the .DLL routine to NOT adjust the PRF value; rather adjust ONLY the IF Bandwidth. This is the default setting. 0 (False) Adjust both the PRF and IF Bandwidth values as necessary. |
Return Type |
Not Applicable |
Default |
Not Applicable |
Example |
|
C++ Syntax |
HRESULT ConfigEnhancedNB(double *pPRF, long *pBW, double *pIF, double *pNCO, double *pStg1, double *pStg2, double *pStg3) |
Interface |
AgilentPNAPulsed.Application |