Write-only |
About Path Configuration |
Description |
Copies the mechanical switch and attenuator settings from the specified channel to the calling channel. To avoid potential conflicts, all port couplings in the calling channel will be turned OFF and all port attenuator settings will be set to manual before copying the switch or attenuator settings. The two channels CAN be of different measurement classes. Use CopyToChannel to copy ALL settings from one channel to another. |
VB Syntax |
pathConfig.CopyFrom (chanNum) |
Variable |
(Type) - Description |
|
pathConfig |
A PathConfiguration (object) |
|
chanNum |
(long integer) Channel number to copy to the calling channel. |
Return Type |
None |
Default |
Not Applicable |
Examples |
Dim chan,pathConfig Set chan = app.ActiveChannel Set pathConfig = chan.PathConfiguration pathConfig.CopyFrom 2 |
C++ Syntax |
HRESULT CopyFrom(long chanNum); |
Interface |
IPathConfiguration2 |
Last modified:
|
3-May-2011 |
New topic |