Write-only |
About Measurement Parameters |
Description |
This method creates a new S-Parameter measurement in an existing or new window. |
VB Syntax |
app.CreateSParameter chan,recvr,source,[window] |
Variable |
(Type) - Description |
|
app |
Application (object) |
|
chan |
(long integer) - Channel number of the new measurement |
|
recvr |
(long integer) - Port number of the receiver (1 or 2) |
|
source |
(long integer) - Port number of the source (1 or 2) |
|
window |
(long integer) - Optional argument. Window number of the new measurement. Choose 1 to 4. If unspecified, the S-Parameter will be created in the Active Window. |
Return Type |
Not Applicable |
Default |
Not Applicable |
Examples |
app.CreateSParameter 1,2,1,1 'Creates a new S21 measurement in channel 1 and New window(1) app.CreateSParameter 1,2,1 'Creates a new S21 measurement in channel 1 and in the active window |
C++ Syntax |
HRESULT CreateSParameter(long ChannelNum, long RcvPort, long SrcPort, long windowNumber) |
Interface |
IApplication |
Last Modified:
|
7-Nov-2013 |
No longer superseded. Use instead of Create SParameterEX Method |