Write-only |
About Measurement Parameters |
Description |
Note: This method is replaced by Create SParameter method. The Load port selection is no longer necessary. Creates a new S-Parameter measurement in an existing or new window and specifies the load port for 3-port devices. |
VB Syntax |
app.CreateSParameterEx chan,recvr,source[,loadPort][,window] |
Variable |
(Type) - Description |
|
app |
Application (object) |
|
chan |
(long integer) - Channel number of the new measurement. |
|
recvr |
(long integer) - Port number of the test port receiver. |
|
source |
(long integer) - Port number of the source. Note: If the port is defined by a string name, such as an external source, a balanced port, or one of the Source 2 outputs on the 2-port 2-source PNA-x model, then you must use chan.getPortNumber to translate the string into a port number. To learn more see Remotely Specifying a Source Port. |
|
loadPort |
(long integer) - Port number of the load. Required for reflection measurements of 3-port devices on multiport PNA models. |
|
window |
(long integer) - Optional argument. Choose between 1and the maximum number of windows allowed on the PNA.. See also Traces, Channels, and Windows on the PNA. If unspecified, the S-Parameter will be created in the Active Window. |
Return Type |
Not Applicable |
Default |
Not Applicable |
Examples |
app.CreateSParameterEx 1,2,1,1 'Creates a new S21 measurement in channel 1 and New window(1) |
C++ Syntax |
HRESULT CreateSParameterEx(long ChannelNum, long RcvPort, long SrcPort, long LoadPort, long windowNumber) |
Interface |
IApplication |
Last modified:
|
14-Dec-2010 |
Deprecated per JE. |
|
24-Apr-2008 |
Modified string names note |
|
9/12/06 |
Modified for number of windows |