Write-only
About Markers

DeleteMarker Method


Description

Deletes a marker from the measurement.

 VB Syntax

meas.DeleteMarker(Mnum)

Variable

(Type) - Description

meas

A Measurement (object)

Mnum

(long) - Any existing marker number in the measurement

Return Type

Not Applicable

Default

Not Applicable

Examples

meas.DeleteMarker(1)

C++ Syntax

HRESULT DeleteMarker(long lMarkerNumber)

Interface

IMeasurement