Write only

DiscardChanges Method


Description

Cancels changes that have been made to the Converter setup and reverts to the previously-saved setup. Same as the Cancel button on the mixer setup dialog box.

 VB Syntax

conv.DiscardChanges

Variable

(Type) - Description

conv

A Converter Object

Return Type

Not Applicable

Default

Not Applicable

Examples

conv.DiscardChanges

C++ Syntax

HRESULT DiscardChanges();

Interface

IConverter