Write-only | 
About Frequency Span | 
Description | 
 Sets the frequency span to the entire frequency span of the analyzer.  | 
VB Syntax | 
 chan.FrequencySpanFull  | 
Variable | 
(Type) - Description | 
| 
 chan  | 
 (object) - A Channel object  | 
Return Type | 
 None  | 
Default | 
 Maximum frequency span of the analyzer  | 
Examples | 
 chan.FrequencySpanFull  | 
C++ Syntax | 
 HRESULT FrequencySpanFull ( );  | 
Interface | 
 IChannel25  |