Description |
This property replaces Get ECALModuleInfo Method. Returns the following information about the connected ECAL module: model number, serial number, connector type, calibration date, min and max frequency. The characterization within the ECal module that this information will be read from is specified by ECALCharacterizationEx. The default value is 0. |
VB Syntax |
moduleInfo = cal.GetECALModuleInfoEx (module) |
Variable |
(Type) - Description |
|
moduleInfo |
(string) - variable to store the module information |
|
cal |
A Calibrator (object) |
|
module |
(long integer) ECal module. Choose from modules 1 through 8 Use IsECALModuleFoundEx to determine the number of modules connected to the PNA |
Return Type |
String |
Default |
Not Applicable |
Examples |
info = cal.GetECALModuleInfoEx(2) Example return string: ModelNumber: 85092-60007, SerialNumber: 01386, ConnectorType: N5FN5F, PortAConnector: Type N (50) female, PortBConnector: Type N (50) female, MinFreq: 30000, MaxFreq: 9100000000, NumberOfPoints: 250, Calibrated: July 4 2002 |
C++ Syntax |
HRESULT GetECALModuleInfoEx(long moduleNumber, BSTR* info); |
Interface |
ICalibrator4 |