Description |
This property replaces ECALCharacterization Property. Specifies the characterization data within an ECal module to be used for the calibration. Learn more about ECal User Characterization. |
VB Syntax |
cal.ECALCharacterizationEx (module) = value |
Variable |
(Type) - Description |
|
cal |
Calibrator (object) |
|
module |
(long integer) Optional argument. ECal module. Choose from modules 1 through 8 Use IsECALModuleFoundEx to determine the number of modules connected to the PNA Use GetECALModuleInfoEx to returns the model and serial number of each module. |
|
value |
(Long) – Characterization data within the ECal module to be used for ECal operations. Choose from: 0 – Factory Characterization 1 – UserCharacterization1 2 – UserCharacterization2 ..and so forth up to... 12 – UserCharacterization12 |
Return Type |
Long |
Default |
0 - Factory Characterization |
Examples |
cal.ECALCharacterizationEx (4) = 2 |
C++ Syntax |
HRESULT put_ECALCharacterizationEx( long moduleNumber, long characterization); HRESULT get_ECALCharacterizationEx( long moduleNumber, long* characterization); |
Interface |
ICalibrator4 |
Last Modified:
|
15-Jun-10 |
Updated for 12 User chars |