Read-only
About Trigger

GetNumberOfGroups Method


Description

Returns the number of groups a channel has yet to acquire.  To set the number of groups for a channel, use Number Of Groups Method

 VB Syntax

value = chan.GetNumberOfGroups

Variable

(Type) - Description

value

(Long Integer) - Number of groups

chan

Channel (object)

Return Type

(Long Integer)

Default

Not Applicable

Examples

groups = chan.GetNumberOfGroups 'Read

C++ Syntax

HRESULT GetNumberOfGroups(long* numberOfGroups);

Interface

IChannel3