Read-only |
About Cal Sets |
Description |
Returns standard acquisition data from the Cal Set. The returned data is complex pairs. Learn more about Reading and Writing Cal Data |
VB Syntax |
data = calSet.GetStandardByString(stdName) |
Variable |
(Type) - Description |
|
data |
(Variant) Two-dimensional safe array to store the returned data. Memory for the returned Variant is allocated by the PNA and must be released by client. Note: See also Get StandardComplexByString on the ICalData2 interface to avoid using the variant data type. |
|
calSet |
A CalSet (Object) |
|
stdName |
(String) The string used to identify a particular standard in the Cal Set. An example string requesting the data for the Load standard in a full 2 port cal might be "S11C(3,3)". |
Return Type |
Variant |
Default |
Not Applicable |
Examples |
See an example |
C++ Syntax |
HRESULT GetStandardByString( BSTR bufferName, VARIANT* pdata) |
Interface |
ICalSet2 |