Write-only |
About LXI |
Description |
Performs an initialization (reset) of the PNA’s LAN configuration, as dictated by Section 8.14 of the LAN eXtensions for Instrumentation (LXI) standard (Version 1.1). This performs the same operation as pressing the LAN Reset button on the PNA LAN Status dialog. |
VB Syntax |
app.LANConfigurationInitialize |
Variable |
(Type) - Description |
|
app |
An Application (object) |
Return Type |
Not Applicable |
Default |
Not Applicable |
Examples |
app.LANConfigurationInitialize |
C++ Syntax |
HRESULT LANConfigurationInitialize (); |
Interface |
IApplication13 |