PNA-X, N522x, and PNA-C models that were shipped with PNA version A.08.20 or higher are LXI-1.1 and VXI-11.3 compliant.
A PNA is LXI-1.1 compliant if the
logo appears on the dialog box shown below.
Learn more about LXI at http://www.lxistandard.org/
To be compliant with VXI-11.3, the PNA must have been either:
Shipped from the factory with PNA version A.08.20 or higher, or
Had the Hard Disk Drive (HDD) upgraded since about June 2008 when A.08.20 was released and using PNA Rev. A.08.20 or higher.
Learn more about VXI at http://www.vxi.org/
When a LAN connection is used with the PNA, the LAN Status dialog allows you to see the IP address and other LAN connection properties.
|
Indicator Shows the current status of the LAN connection. NORMAL - Indicates that the PNA LAN is ready for communication. IDENTIFY - Indicates that a remote computer has invoked an LXI identification operation on the PNA using the web-based interface or LXIDeviceIDState COM property. FAULT - Indicates that the PNA LAN interface is not connected to the Internet. IP Address Shows the current IP address of the PNA Computer Name Shows the full computer name of the PNA. Learn how to change this. If you see the IP address listed here, that means there is no DNS server specified in the network setup. MAC Address Shows the unique address of the PNA computer. Also known as HostID. LAN Reset Provides a LAN Configuration Initialize (LCI) mechanism. Press to return the following settings to factory default conditions:
|
If your PNA is LXI Class C compliant (see above), you can connect to the PNA using a web browser over an internet connection.
To do this, when the above dialog indicates a NORMAL condition:
From a web browser, type http://<your_PNA_computer_name>. For example, to connect to the fictitious PNA in the dialog above, type: http://pna1-22
Type the log on User Name and Password
You will see the following welcome screen with connection links.