Write-only |
About Cal Sets |
Description |
Adds stimulus data to the specified buffer. The size of vdata must agree with the size of the complex data already attached to the buffer or an error will be generated. See Also: GetErrorTermStimulus Method Learn more about Reading and Writing Cal Data |
VB Syntax |
calSet.PutErrorTermStimulus(bufferName, vdata) |
Variable |
(Type) - Description |
|
calSet |
(Object) A CalSet Object |
|
bufferName |
(String) The string name used to identify a particular error term in the Cal Set. An example string for port 3 directivity in a full 2 port cal might be "Directivity(3,3)". To determine the string names of error terms, see GetErrorTermList2. |
|
vdata |
(Variant) Safearray of variants (doubles). |
Return Type |
Not Applicable |
Default |
Not Applicable |
Examples |
The sequence is: complexData = calset1.GetErrorTermByString(0, BufferName) frequencyData = calset1.GetErrorTermStimulus(0,BufferName) // manipulate complex data here Calset2.PutErrorTermByString(BufferName, manipulatedComplexData) Calset2.PutErrorTermStimulus(BufferName, frequencyData); |
C++ Syntax |
HRESULT PutErrorTermStimulus (BSTR bufferName, VARIANT vardata) |
Interface |
ICalSet7 |
Last modified:
|
2-May-2011 |
New topic |