Write-only
About Cal Sets

PutErrorTermComplexByString Method


Description

Puts error term data into the Cal Set.

Learn more about Reading and Writing Cal Data

See examples of Reading and Writing Cal Set Data

 VB Syntax

ICalData3.PutErrorTermComplexByString errorName, lnumPoints, real(0), imag(0)

Variable

(Type) - Description

ICalData3

An ICalData3 pointer to a Cal Set object.

errorName

(String) The string name used to identify a particular error term in the Cal Set.  An example string for port 3 directivity in a full 2 port cal might be "Directivity(3,3)". To determine the string names of error terms, see GetErrorTermList2.

lnumPoints

(Long)  The number of data points in the real and imaginary arrays.

real

(Single) The real component of the complex data.

imag

(Single) The imaginary component of the complex data.

Note: The size of the real and imaginary arrays should be the same.

Return Value

Not Applicable

Default

Not Applicable

Examples

See example

C++ Syntax

HRESULT PutErrorTermComplexByString( BSTR bufferName, long  lnumPoints, float* real, float* imag);

Interface

ICalData3