Write-only
About Cal Sets

PutStandardByString


Description

Puts standard acquisition data into the Cal Set.

Learn more about Reading and Writing Cal Data

See examples of Reading and Writing Cal Set Data.

 VB Syntax

PutStandardByString(stdName, vdata)

Variable

(Type) - Description

stdName

(String) The string used to identify a particular standard in the Cal Set.  An example string requesting the data for the Load standard in a full 2 port cal might be "S11C(3,3)".

vdata

(Variant) The variant containing a safearray of variants.  This data is usually two dimensional.

Note: The vardata array is a safearray of variants wrapped in a variant.  This structure is compatible with scripting clients who can only use variants.  For alternative methods that used typed arrays, see ICalData3.

Return Type

Not Applicable

Default

Not Applicable

Examples

See an Example

C++ Syntax

HRESULT PutStandardByString(   BSTR bufferName,  VARIANT vardata);

Interface

ICalSet2