Write-only

Quit Method


Description

Terminates the Network Analyzer application.

 VB Syntax

app.Quit

Variable

(Type) - Description

app

An Application (object)

Return Type

Not Applicable

Default

Not Applicable

Examples

app.Quit

C++ Syntax

HRESULT Quit()

Interface

IApplication

Remarks

Under the rules of COM, the server should not exit until all references to it have been released. This method is a brute force way of terminating the application. Be sure to release all references (or terminate the client program) before attempting to restart the Network Analyzer application.

An alternate approach to terminating the application is to make the application invisible (app.Visible = False) and release all references. The server will shutdown.