Write-only
About Independent Power Calibration

Reset (Independent CalAll) Method


Description

This command resets all ranges for the given source port <n>.

 VB Syntax

IndependentPwrrCal.Reset

Variable

(Type) - Description

IndependentPwrrCal

A IndependentPowerCalibration (object)

Return Type

Not Applicable

Default

Not Applicable

Example

CalibrateAllChannels.IndependentPowerCalibration(3).Reset

C++ Syntax

HRESULT Reset

Interface

IIndependentPowerCalibration