Write-only
About Cal Window

SetupMeasurementsForStep Method


Description

Show the Cal Window, and optionally one or more other specific windows, before acquiring a Cal standard. This command will cause the Cal Window to display the specific measurements that are to be made for that particular Cal standard.

See custom Cal window commands.

 VB Syntax

guidedCal.SetupMeasurementsForStep (n)

Variable

(Type) - Description

guidedCal

A GuidedCalibration (object)

n

Step number in the calibration process.

Use GenerateSteps to determine the total number of steps.

Use GetStepDescription to read the description of each step.

Return Type

Not Applicable

Default

Not Applicable

Examples

guidedCal.SetupMeasurementsForStep 3

See example using this command

C++ Syntax

HRESULT SetupMeasurementsForStep(long step);

Interface

IGuidedCalibration4