Write-only
About Trace Hold

TraceHoldClear Method


Description

Resets the currently-stored data points to the live data trace and restarts the currently-selected Trace Hold type.

VB Syntax

meas.TraceHoldClear ()

Variable

(Type) - Description

Return Type

Not Applicable

Default

Not Applicable

Examples

meas.TraceHoldClear

C++ Syntax

HRESULT TraceHoldClear( );

Interface

IMeasurement16