Write-only |
About User Preset |
Description |
Loads an existing instrument state file (.sta or .cst) to be used for User Preset. Subsequent execution of app.UserPreset will cause the PNA to assume this instrument state. Regardless of the state of the User Preset Enable checkbox, the app.Preset command will always preset the PNA to the factory preset settings, and app.UserPreset will always perform a User Preset. |
VB Syntax |
app.UserPresetLoadFile (file) |
Variable |
(Type) - Description |
|
app |
An Application (object) |
|
file |
(String) Full path, name, and extension of the file to be loaded. |
Return Type |
Not Applicable |
Default |
Not Applicable |
Examples |
app.UserPresetLoadFile ("C:/Program Files/Keysight/Network Analyzer/Documents/10MHzto20GHz.sta") |
C++ Syntax |
HRESULT UserPresetLoadFile (BSTR bstrFile) |
Interface |
IApplication6 |