Read-only |
|
Description |
This command is replaced with get InputVoltageEX Method Reads the ADC input voltage from Analog IN (pin 14) of the AUX IO connector. For PNA |
VB Syntax |
volts = AuxIO.get_InputVoltage |
Variable |
(Type) - Description |
volts |
(double) - variable to store the return value |
AuxIO |
(object) - A Hardware Auxiliary Input / Output object |
Return Type |
Double |
Default |
0 |
Examples |
Dim aux as HWAuxIO Set aux = PNA.getAuxIO |
C++ Syntax |
HRESULT get_InputVoltage ( double* Voltage ); |
Interface |
HWAuxIO |