Read-only |
|
Description |
This command replaces get InputVoltage Method Reads the ADC voltage from the specified location. |
VB Syntax |
volts = AuxIO.InputVoltageEX loc |
Variable |
(Type) - Description |
|
volts |
(double) - variable to store the return value |
|
AuxIO |
(object) - A Hardware Auxiliary Input / Output object |
|
loc |
(Long) Location from which to read data. For PNA-X models:, reads ADC voltages from the Power I/O connector. Choose from: 1 Reads voltage on Analog In 1 port (pin 7). 2 Reads voltage on Analog In 2 port (pin 8). 3 Reads voltage on GndSens (pin 6). 4 Reads voltage on Analog Out 1 port (pin 3). 5 Reads voltage on Analog Out 2 port (pin 4). For all other PNA models: 1 Reads voltage on the Analog IN (pin 14) of the AUX IO connector. 4 Reads voltage on Analog Out 1 port (pin 3). 5 Reads voltage on Analog Out 2 port (pin 2). |
Return Type |
Double |
Default |
Not Applicable |
Examples |
Dim aux as HWAuxIO Set aux = PNA.getAuxIO 'for PNA-X, read voltage on PowerI/O pin 7 'for all other models, reads voltage on Aux I/O Analog In (pin 14) |
C++ Syntax |
HRESULT get_InputVoltageEX (long muxLoc, double* vtVoltage ); |
Interface |
HWAuxIO2 |