Write-only |
|
Description |
E836x and PNA-L: Sets voltages on the DAC/Analog Output 1|2 of the Auxiliary IO connector. PNA-X: Sets voltage on the Power I/O connector AnalogOut1|2. Read output voltages using get OutputVoltage Method. |
VB Syntax |
AuxIO.put_OutputVoltage output, voltage |
Variable |
(Type) - Description |
AuxIO |
(object) - A Hardware Auxiliary Input / Output object |
output |
(variant) Number of the output DAC to write voltage to. Choose from: 1 Output 1 (Aux I/O pin 3) and (Power I/O pin 3) 2 Output 2 (Aux I/O pin 2) and (Power I/O pin 4) |
voltage |
(double) Voltage to write to the output DAC. Choose a voltage from -10 to 10 |
Return Type |
None |
Default |
None |
Examples |
HWAuxIO.put_OutputVoltage 1,9 'set Analog Out1 to +9v |
C++ Syntax |
HRESULT put_OutputVoltage (VARIANT Output, double Voltage ); |
Interface |
IHWAuxIO |