CalFactorSegmentsPMAR Collection


Description

A collection object that provides a mechanism for iterating through the segments of a power sensor cal factor table. The Cal Factor table can contain up to 100 segments. This collection is used when the Power Meter is used as a Receiver.

Accessing the CalFactorSegmentsPMAR collection

Example: Create a PMAR Device and Measurement

See Also:

 

Methods

Description

Add

Adds a PowerSensorCalFactorSegmentPMAR object to the collection

Item

Use to get a handle to a PowerSensorCalFactorSegmentPMAR object in the collection.

Remove

Removes an PowerSensorCalFactorSegmentPMAR object from the collection.

Properties

Description

Count

Returns the number of PowerSensorCalFactorSegmentPMAR objects in the collection.

Parent

Returns a handle to the Parent object of this collection.