Write-only |
Description |
Returns an object from the collection of objects. Notes
|
VB Syntax |
Object[.Item](n) |
Variable |
(Type) - Description |
|
Object |
Any of the following (collections): |
|
.Item |
Optional - Item is the default property of a collections object and therefore can be called implicitly. For example, the following two commands are equivalent: Channels.Item(3).Averaging = 1 |
|
n |
(variant) - Number of the item in the collection. In addition, the following collections allow you to specify the name of the item as a string:
|
Return Type |
(Object) |
Default |
Not Applicable |
Examples |
For i = 1 to Traces.Count 1 |
C++ Syntax |
HRESULT Item(VARIANT index, <interface>** pItem) |
Interfaces |
All listed above. |
Last Modified:
|
15-Sep-2014 |
Specify the collections that allow naming |
|
8-Feb-2011 |
Added GuidedCalibrationPowerSensors |
|
10-Sep-2008 |
Added CalSets name note |