Write-only |
Description |
Removes an item from a collection of objects. |
VB Syntax |
Object.Remove item |
Variable |
(Type) - Description |
|
Object |
Any of the following (objects) Note: Segments, CalFactorSegments, and PowerLossSegments have an OPTIONAL argument [size] referring to the number of segments to remove, starting with the item parameter. Note: Segments - When ALL segments are deleted, SweepType is automatically set to Linear because there are no segments to sweep. |
|
item |
(variant) - Collection Item number to be removed. Note: The ExternalDevices Collection requires that you specify item as the string name of the device. For example: |
Return Type |
Not Applicable |
Default |
Not Applicable |
Examples |
Measurements.Remove 3 'Removes the third measurement in the collection segments.Remove 2,20 'Removes 20 segments (2 - 21) |
C++ Syntax |
HRESULT Remove(VARIANT index); //Measurements HRESULT Remove(VARIANT index); //Cal Sets HRESULT Remove(long windowNumber); //NAWindows HRESULT Remove(VARIANT index, long size); //Segments HRESULT Remove(VARIANT index, long size); //CalFactorSegments(PMAR) HRESULT Remove(VARIANT index, long size); //PowerLossSegments(PMAR) HRESULT Remove(BSTR name) //ExternalDevices HRESULT Remove( VARIANT index) // Channels - specify collections index, not the channel number. HRESULT Remove(VARIANT index); //GuidedCalibrationPowerSensors |
Interface |
All listed above |
Last Modified:
|
8-Feb-2011 |
Added GuidedCalibrationPowerSensors (9.33) |
|
16-Sep-2010 |
Added channels (9.30) |
|
31-Jul-2009 |
Added External Devices (9.0) |