Description
ExternalDevice objects allow you to set properties and methods for each external device.
Obtain a handle to an External Device by specifying an item in the External Devices collection.
Although the following example shows how to create a PMAR external device, you can substitute any supported external device for "PMAR" and DeviceType: "Power Meter".
|
dim app Set app = CreateObject("AgilentPNA835x.Application") dim externalDevices Set externalDevices = app.ExternalDevices dim devicecount devicecount = externalDevices.count externalDevices.Add "NewPMAR" dim newExternalDevice Set newExternalDevice = externalDevices.Item("NewPMAR") newExternalDevice.DeviceType = "Power Meter" newExternalDevice.IOConfiguration= "GPIB0::14::INSTR" newExternalDevice.IOEnable = true
|
Learn how to Configure an External Device
Methods |
Interface |
Description |
|---|---|---|
|
IExternalDevice2 |
Recalls an external device configuration file from the PNA hard drive. Currently, only DC Meter and DC Supply devices are supported. |
|
|
IExternalDevice2 |
Saves an external device configuration file to the PNA hard drive. Currently, only DC Meter and DC Supply devices are supported. |
|
Properties |
|
Description |
|
IExternalDevice |
Sets and returns the state of activation for an external device. |
|
|
IExternalDevice |
Sets and returns the DeviceType (source, power meter) for the external device. |
|
|
IExternalDevice |
Sets and returns the external device driver (model). |
|
|
IExternalDevice |
Provides access to properties that are unique to the external device type. |
|
|
IExternalDevice |
Sets and returns the method of communication and address for the external device. |
|
|
IExternalDevice |
Sets and returns whether an external device is available for IO communication with the PNA. |
|
|
IExternalDevice |
Sets and returns the name of the External Device. |
|
|
IExternalDevice |
Sets and returns the time out value for communication with the external device. |
|
Interface |
Introduced with PNA Rev: |
|
IExternalDevice |
9.0 |
|
IExternalDevice2 |
9.50 |
Last Modified:
|
14-Mar-2012 |
Added links to other device types |
|
31-Jul-2009 |
MX New topic (9.0) |