Write-only

ExtendedProperties Property


Description

Provides access to the custom properties and methods of an external device.

 VB Syntax

Set PSG = ExtDev.ExtendedProperties

Variable

(Type) - Description

PSG

(Object) Variable to store the returned handle to an external device.

ExtDev

An ExternalDevice (object)

Return Type

Object

Default

Not Applicable

Examples

See Example

C++ Syntax

HRESULT get_ExtendedProperties(IDispatch** ppObject);

  Interface

IExternalDevice