Write-only |
About Arrange Windows |
Description |
Sets the arrangement of all the windows. Overlay, Stack2, Split3 and Quad4 will create windows. To control the state of one window, use app.WindowState. |
VB Syntax |
app.ArrangeWindows = value |
Variable |
(Type) - Description |
|
app |
An Application (object) |
|
value |
(enum NAWindowModes) - Choose from: 0 - naTile |
Return Type |
Not Applicable |
Default |
naTile |
Examples |
app.ArrangeWindow = naTile 'Write |
C++ Syntax |
HRESULT put_ArrangeWindows(tagNAWindowModes newVal) |
Interface |
IApplication |