Write/Read
About SA Application

AutoBandwidth Property


Description

Set and read the default values for DFT bandwidth.

VB Syntax

sa.dft.AutoBandwidth = value

Variable

(Type) - Description

sa.dft

A SpectrumAnalyzerDFT (object)

value

(Boolean) Choose from:

0 - OFF - DFT minimum and maximum values are set manually:

Narrow - 500 kHz to 11 MHz

Wide - 500 kHz to 44 MHz

1 - ON - DFT minimum and maximum values are set to their default values:

Narrow - 1 MHz to 10 MHz

Wide - 1 MHz to 34 MHz

Return Type

Boolean

Default

1

Examples

sa.dft.AutoBandwidth = 0  'Write

bwidth = sa.dft.AutoBandwidth 'Read

C++ Syntax

HRESULT put_AutoBandwidth(VARIANT_BOOL bEnable);

HRESULT get_AutoBandwidth(VARIANT_BOOL* bEnable);

Interface

ISpectrumAnalyzerDFT