In this topic:
Spectrum Analyzer mmWave Measurements
Spectrum Analyzer Option 090
Windows 7 operating system
Option 092 (10 MHz to ≤ 90 GHz) for broadband spectrum analyzer millimeter-wave measurements
Option 093 (10 MHz to ≤ 110 GHz) for broadband spectrum analyzer millimeter-wave measurements
Option 094 (> 110 GHz) for banded spectrum analyzer millimeter-wave measurements
IF Response Adjustment required after installing Option 090, 092, 093, or 094
Configure SA settings.
Set up the SA source frequency and power.
Define the measurement parameters.
Select markers.
Calibrate the SA channel using the Cal All wizard.
On the PNA front panel, press Meas > Measurement Class....
Select Spectrum Analysis, then either:
OK delete the existing measurement, or
New Channel to create the measurement in a new channel.
A Spectrum Analysis measurement is displayed.
Configure SA settings |
|
Using front-panel |
Using Menus |
|
|
Sweep Type - Sets the spectrum analysis sweep type. See Type (Sweep). Processing Resolution Bandwidth - Provides the ability to resolve, or see closely spaced signals. The narrower (lower) the Resolution Bandwidth, the better the spectrum analyzer can resolve signals. In addition, as the Resolution Bandwidth is narrowed, less noise is measured by the spectrum analyzer ADC and the noise floor on the display lowers as a result. This allows low level signals to be seen and measured. However, as the Resolution Bandwidth is narrowed, the sweep speed becomes slower. Auto - Check to couple Resolution Bandwidth to the frequency span in a ratio based on the Span/RBW setting. As the frequency span is narrowed, the Resolution Bandwidth is also narrowed providing increased ability to resolve signals. Clear to uncouple the settings. Video Bandwidth - Sets the video averaging factor. The averaging operation is applied after the DFT (Discrete Fourier Transform) and before the image rejection. The trace data is smoothed with the method selected by the Video Averaging Type. More smoothing occurs as the Video BW is set lower. However, as the Video BW is narrowed, the sweep speed becomes slower. The Video Bandwidth can be set from 3 Hz to 3 MHz when Auto is deselected. Auto - Check to couple the Resolution Bandwidth to the Video Bandwidth in a ratio based on the RBW/VBW setting. Clear to uncouple the settings. Detector Type - A "detector" is an algorithm used to map DFT bins into display buckets. There are typically several DFT bins in a single display bucket, and the detector determines how to translate the multiple DFT values into a single display value. Peak - Displays the maximum value of all the measurements in each bucket. This setting ensures that no signal is missed. However, it is not a good representation of the random noise in each bucket. Average - Displays the Root Mean Squared (RMS) average power of all the measurements in each bucket. This is the preferred method when making power measurements. Sample - Displays the center measurement of all the measurements in each bucket. This setting gives a good representation of the random noise in each bucket. However, it does not ensure that all signals are represented. Normal - Provides a better visual display of random noise than Positive peak and avoids the missed-signal problem of the Sample Mode. Should the signal both rise and fall within the bucket interval, then the algorithm classifies the signal as noise. An odd-numbered data point displays the maximum value encountered during its bucket. An even-numbered data point displays the minimum value encountered during its bucket. If the signal is NOT classified as noise (does NOT rise and fall) then Normal is equivalent to Positive Peak. NegPeak- Displays the minimum value of all the measurements in each bucket. Peak Sample - Attempts to determine if the display bucket contains an actual signal, or just noise. If a signal is present, the Peak detector is used, otherwise Sample is applied. Peak Average - Attempts to determine if the display bucket contains an actual signal, or just noise. If a signal is present, the Peak detector is used, otherwise Average is applied. Bypass - Check to bypass the Detector Type to view all display points from the DFT. This is only available if the total number of DFT points of the current span can be handled by the display. Averaging Type - Determines how to compute the video average. When Auto is selected, the optimum type of averaging for the current instrument measurement settings is selected. It averages the magnitude of the DFT bins. Averaging only applies if the video bandwidth is less than the resolution bandwidth. Voltage - Selects averaging of the detected signal's magnitude and returns the result. Power - Selects averaging of the detected signal's squared magnitude and returns the square root of the result. Log - Selects averaging of the detected signal's natural logarithm of the magnitude and returns the exponentiated value of the result. Voltage Max - Returns the maximum voltage (signal magnitude) measured during the averaging period. Voltage Min - Returns the minimum voltage (signal magnitude) measured during the averaging period. Averaging Count - Reads the number of Video bandwidth sweeps that are averaged together. This readout is displayed to the right of the Averaging Type selection (the small "1" shown in the dialog above). It can be read with the remote interface using the SENS:SA:BAND:VID:AVER:COUNt? command. Sets the SA (receiver) frequency range when running Linear Frequency sweep type. Use either of the following pairs of settings to determine the frequency range. Start /Stop - Specifies the beginning and end frequency of the swept receiver range. Start is the beginning of the X-axis and Stop is the end of the X-axis. When the Start and Stop frequencies are entered, then the X-axis annotation on the screen shows the Start and Stop frequencies. Center /Span - Specifies the value at the center and frequency range. The Center frequency is at the exact center of the X-axis. The Frequency Span places half of the frequency range on either side of center. When the Center and Frequency Span values are entered, then the X-axis annotation on the screen shows the Center and Span frequencies. Number of Points - Selects the number of trace points on the display. When the Detector is bypassed, the number of display points is read only, it shows the current DFT points to cover the RF span. Note: When running Segments, the frequency ranges are set by the segment table. AttenuatorsReceiver Attenuation is used to protect the test port receivers from damage or compression. Receiver attenuation causes the applied power at the receiver to be less than the power at the test port by the specified amount of attenuation. Receiver Attenuators are offered as an option. Learn more. Type or select independent attenuation values for each test port receiver. A preference can be set to mathematically offset (or NOT) the reported power at the test port receivers by the amount of receiver attenuation. By default, All PNA models offset the display. Learn how to set the preference.
|
|
Power On (All Channels) Check to enable source power for all channels. Only turns power ON if the port State setting is ON. Port Powers Coupled
Source Cells Name - Lists the test ports through which an internal source is available. If an external source has been configured, it will appear at the bottom of the list. State
CW - The source is set to a CW frequency. LinFreq - The source is set to sweep from the Start to Stop frequency. Power - The source is set to a power sweep. LinF+Pwr - The source is set to sweep from the Start to Stop frequency and power sweep. The order is determined by the Sweep Order selection below. Segments - The source is set to sweep in frequency sub-sweeps. For each segment you can define independent power levels, IF bandwidth, and sweep time. Frequency - Click in the cell, then click Edit, to start the Frequency Settings dialog (below). Power - Sets the power level at the output of the source. Click in the cell, then click Edit, to start the Power Settings dialog (below). Modulation - Choose from OFF, ON, Pulse. If Enable Modulation Control is enabled, an external modulation source can be controlled (turn on and off its modulation state). RF Sweep OrderThe following settings apply only when LinF+Pwr is selected as the Type of sweep. Frequency First - Sweep from Start to Stop frequency first followed by a power sweep. Power First - Sweep power first then sweep from Start to Stop frequency. ButtonsPath Configuration Learn more Pulse Setup Learn more External Devices Learn more Power and Attenuator Learn more |
|
Properties RBW Shape - Selects the digital filter (window) to apply to the time domain IF signal. The filter effectively "shapes" the signal before application of the DFT to help avoid discontinuities which add unwanted frequency content to the spectrum. Each filter has its own advantages and disadvantages. Gaussian - Selects a Gaussian window. The Gaussian window has good frequency separation and moderate amplitude accuracy. This window provides higher dynamic range because it has much lower side lobes. It is used for general-purpose measurements and when high dynamic range is required. Flat Top - Selects the flat top window for amplitude measurement of sinusoidal frequency components. The flat top window has moderate frequency separation and excellent amplitude accuracy. It is typically used for narrowband signals when measuring the amplitude of a particular frequency component with greater amplitude accuracy. Kaiser - Selects the Kaiser window which is an approximation of a Slepian window using Bessel functions. This window has a relatively high dynamic range and is similar to the Blackman window. Blackman - Selects the Blackman window. This window has a relatively high dynamic range and is similar to the Kaiser window. No Window - The No Window selection does not modify the time-domain data in any way before applying an DFT. This selection is very fast but may yield a significant number of side lobes in the frequency domain because of spectral leakage. This selection has a rectangular shape and does not attenuate any portion of the time record. Image Reject Type - Sets the minimum number of distinct DFT acquisitions to use when computing an actual signal. As the number of DFT acquisitions increases from the None, LO Low setting to the Max setting, an increased number of erroneous signals are eliminated. Therefore, the Better and Max settings provide the highest confidence that what remains are actual signals, at the expense of slower measurements. None, LO High - Selects 1 acquisition with the LO higher than the receiver frequency. Note: Selecting None, LO High with a span reaching the high end frequency of the PNA is not possible. See SA Warning Messages. None, LO Low - Selects 1 acquisition with the LO lower than the receiver frequency. Note: Selecting None, LO Low with a span reaching the low end frequency of the PNA is not possible. See SA Warning Messages. Min - Selects 2 acquisitions. Normal - Selects 4 acquisitions. Better - Selects 6 acquisitions. Max - Selects 8 acquisitions. Image Reject Strength - Sets the image rejection strength. During the image rejection process, several LO acquisitions overlap at the same RF frequency (depending on the Image Reject Type). As a result, different RF signal values can be returned. This feature sets the acceptable power differences between measurements performed with different LOs in determining actual signals. Possible values are Weak, Normal, Strong. Weak accepts more difference between measurements, and strong less difference. RBW/VBW - Sets the ratio of Resolution Bandwidth to Video Bandwidth when the Video Bandwidth is in Auto mode. Span/RBW - Sets the ratio of Span to Resolution Bandwidth when the Resolution Bandwidth is in Auto mode. CF Step Size - Manually sets the amount Center frequency change that occurs when ▲|▼ is clicked (next to the value). Auto - Each press of the ▲|▼ arrows increments or decrements the Center frequency by 5% of the current frequency span. Occupied BW search min - Sets the minimum search frequency to use during an Occupied BW search measurement. Power below this frequency is ignored. See Occupied BW Ratio for information about setting up this measurement type. DC SourcesDC source control allows the spectrum to be measured at multiple DC source settings. Enable DC Outputs - Enables all DC source outputs that are turned ON in the DC Source dialog. This same selection is found in the DC Source Dialog. Enable DC Sweep - Enables the DC sources to sweep between their start and stop voltages. If not selected, then the DC sources will be set to their start voltages. DC Sources... - Configure internal DC sources. Learn more. Number of DC levels - Defines the number of voltage levels in the DC sweep. The following settings apply to the measurement loop order. The SA may be programmed to loop through a series of spectrum measurements at multiple RF source frequencies, multiple RF source powers, and multiple DC voltages. These radio buttons determine whether the DC sources are swept before the RF power and frequencies are swept, or whether the DC sources are swept after the RF power and frequencies are swept. Sweep Order DC before RF - Sweep through each DC voltage step first then sweep through the next frequency. RF before DC - Sweep through each frequency step first then sweep through the next DC voltage. Advanced >> button - Accesses the IF, Trigger, Processing, and ADC & LO, and Data dialogs.
|
|
IF GainAuto - Selects the appropriate amount for gain versus RF frequency bands for each receiver IF Path. Or select a specific amount of gain (in dB) for IF receiver paths. Couple all IF paths - When checked, all receivers assume the same setting. When cleared, each receiver can assume an individual setting. IFConfig - Accesses the IF Path Configuration dialog. Learn all about IF Path Configuration. ADC Filter - Selects between a narrow and wide IF filter anti-aliasing path. Narrow 11MHz - Selects the ADC 11 MHz IF filter path. A warning message will appear if the Narrow IF filter path is selected and the Resolution Bandwidth is > 1 MHz. See SA Warning Messages. Wide 38MHz - Selects the ADC 38 MHz IF filter path. Auto - Check to automatically set the ADC Filter setting based on the ADC Sampling Frequency. DFT Bandwidth Auto - Enables the default values for DFT bandwidth. With Auto checked, the default values are: Narrow - 1 MHz to 10 MHz Wide - 1 MHz to 34 MHz With Auto unchecked, the values can be entered manually. The ranges are: Narrow - 500 kHz to 11 MHz Wide - 500 kHz to 44 MHz
|
|
This Data page is intended to give access to the SA engine data after the Fourier transform, and before the display detection data reduction (peak detector…). In other words, access to the DFT image rejected frequency points. It is still possible to output data from a SA channel with the legacy PNA data output functions, but these functions are tied to the number of display points. Note that the markers, with special peak search, band power, noise power, and occupied band modes are another convenient way to grab data from a SA channel. Float LogMag (dB) - Sets the data format to log magnitude in dBm. Float LinMag - Sets the data format to linear magnitude in volts. Integers - Sets the data format to Packed Integers (each value is a short 16 bit integer, the equation to compute the dBm value is: dBm = Xshort/200.0 - 36.165 Export receivers - Select the data to export from a specific receiver or all receivers. Don't save data below threshold - Set data level threshold mode and threshold level in dBm. For text file output with verbose mode, only the frequencies with power greater than this threshold setting will be written to the file. DFT bins count - Displays the current DFT bin count, the number of DFT points processed across the total RF span. When the Detector is bypassed, this is the number of points that are sent to the display. Receivers count - Displays how many receivers are currently being exported. The number here can be less than the number of receivers specified in Export Receivers, if some of them at not selected in the channel.
Export to binary file - Set data to be exported to a binary file. Data is not exported until the next new sweep occurs. Export to text file - Exports data only. Data is not exported until the next new sweep occurs. Verbose mode - Exports frequency and data. Data is not exported until the next new sweep occurs. Erase files each new sweep - Selecting this option will erase the data after each sweep. If this option is not checked, the data from each sweep will continue to be appended to the output data file which can create a very large file size (and fill the disk, with many unwanted consequences). File name prefix - The receiver selected in Export receivers will be appended to the prefix name specified in this field with either ".txt" if a text file is exported or ".bin" if a binary file is exported. For example, if C:\Temp\SA_DATA_OUT is entered into the File name prefix field and the "B" receiver data is exported to a text file, the data will be exported to a file called SA_DATA_OUT_B.txt. Record size (bytes) - This is the byte size of binary data output. Export markers - Adds marker data to the text file (*.txt) output.
Export to FIFO buffer - Exports data to the FIFO (First-IN, First-OUT) data buffer. FIFO is a circular buffer that allows very fast Read-Write access. Export to shared memory - Exports data to shared memory (Microsoft Windows feature) which is the fastest way to transfer data between applications. The application that is retrieving data has to register itself to Microsoft Windows with the same share name. Share name - Assigns a specified name to the shared data.
|
|
In the SA Setup Source Tab (above): > When (Sweep) Type = CW, set the CW Frequency.
> When (Sweep) Type = Linear, the following dialog appears:
SettingsSets the source frequency range. Use either of the following pairs of settings to set the frequency range. Start /Stop - Specifies the beginning and end frequency of the swept range. Center /Span - Specifies the value at the center and frequency range. Source Number of Steps - Sets the number of steps the source will make across the specified source frequency range. SA Sweeps / Source Step - Sets the number of SA (receiver) sweeps for each Source Step. This setting is common to all sources. |
|
In the SA Setup Source Tab (above): > When (Sweep) Type = CW or LinFreq, set the power level.
> When (Sweep) Type = Power or LinF+Pwr, the following dialog appears:
SettingsSets the source power range. Use either of the following pairs of settings to set the power range. Start /Stop - Specifies the beginning and end power of the swept range. Center /Span - Specifies the value at the center and power range. Source Number of Steps - Sets the number of steps the source will make across the specified source power range. SA Sweeps / Source Step - Sets the number of SA (receiver) sweeps for each Source Step. This setting is common to all sources. |
|
How to select and configure Measurement Parameters |
|
Using front-panel |
Using Menus |
|
|

Select one of the test port receivers to make a measurement. Test ports are identified in both traditional VNA notation and Receiver Notation. Learn more.
Or select an ImageReject measurement, if the Display Image Reject Traces checkbox has been set.
Create in New Window - When checked, the selected measurements are created in a new window.
Select All - Select all measurement parameters.
Clear All - Clear all measurement parameters.
Note: Configuring an external DC meter for a SA channel is supported. DC is read at the end of a sweep. Only one point is read and the entire trace is filled with this point reading regardless of the number of channel points.
The following marker-related features are unique to SA. Marker => SAThis feature is supported in Standard, SMC or Swept IMD measurement classes (channels) ONLY. In this section, these are called NA channels. On a standard channel with a marker residing on a trace in an NA channel, Marker=>SA creates a new SA channel in full frequency span. Refer to the following for swept IMD and SMC: Swept IMD: span = 10 * delta frequency SMC: SA channel uses receiver frequency range A marker is created on the trace at the same frequency as the NA channel marker. This is a quick way to see the frequency spectrum of the NA channel at a specific frequency.
How to use Marker =>SA With a marker residing on a trace in a standard channel...
Band MarkersThe following two marker types provide a readout of the total power or noise within a selectable frequency span. These markers can be used with marker tracking ON. Learn more.
Note: If a Band Power or Band Noise marker is selected, Discrete mode is turned OFF to allow precise measurements over the desired frequency range. The span is marked by vertical dotted lines that appear on either side of the marker. The marker's y-axis value is set to the measured power value.
If a Band Power or Band Noise marker is in Delta mode, the difference between the Band Power or Band Noise marker and the reference marker is displayed with a leading delta symbol.
How to select Band Power or Band Noise
If a Band Power or Band Noise measurement cannot be made, the marker readout will display -999 dBm (for Band Power), or -999 dBm/Hz (for Band Noise). There are two reasons why this may happen:
Occupied BW RatioThe Occupied BW Ratio is the frequency band in the measurement that contains a specific percentage of the total power in the measured frequency span. The marker readout provides the occupied band center frequency, percentage of the band span to measure, and the occupied band power. See also Occupied BW search min for setting the minium frequency to start a search.
The span is marked by vertical dotted lines that appear on either side of the marker indicating the percentage of span. The marker's y-axis value is set to the measured power value.
How to select Occupied BW Ratio
|
|
A calibration can be performed on the SA Channel using the Cal All Wizard when corrected results are required to improve amplitude accuracy.
Note: Calibration is performed over the currently specified spectrum analyzer frequency range only.
Another method of calibration is to import an existing Cal Set. An imported Cal Set must contain the Receiver Response terms for the measurement port on the SA channel. In addition, if the imported Cal Set covers a narrower frequency range than the SA channel, the error terms in the imported Cal Set are extrapolated.
The Cal Plane Manager can be used to characterize adapters, cables, and fixtures used to connect a DUT to the PNA to remove their effects from the measurement. See the detailed procedure.
Gated spectrum analyzer measurements are triggered measurements that capture data for the duration of the active level of the trigger. Thus, only level external triggers can be used (High level, Low level) for gated measurements. Edge triggers can be used to start SA measurements, but will not gate them. It is not recommended to use level triggers to start measurements: if the active level is shorter than the required acquisition time (that depends on the RBW and other settings), then the measurement will abort.
A given SA sweep needs a given number of LOs (this depends mainly on the span and on the Image Reject setting). This number can be retrieved at the SA Processing dialog. Each LO needs one ADC acquisition and the duration of one ADC acquisition can be retrieved at the SA Processing dialog. The time for each LO acquisition is based on the ADC Record Size times the ADC Sampling Frequency (defaults to 10 nsec). For gated SA, it is meaningful to gate each individual ADC acquisition. This can be done with the Trigger Setup dialog, with the external trigger configured per channel (Trigger Scope) in point mode (channel trigger state mode), and Meas Trigger set to Level.
For example, if the ADC Record Size is 663, the time required for a full DFT acquisition would be 663 x 10 nsec = 6.63 usec. As long as the width of the measurement trigger is greater than 6.63 usec, measurement data will be acquired. If the measurement trigger width is set to less than 6.63 usec, then no measurement data will be acquired. If the width of the measurement trigger is much larger, for example 20 usec, then up to 3 ADC acquisitions with 663 samples can occur during the active status of the trigger.
Note: Internal Pulse0 pulse generator is not suitable for gated SA because the pulse width cannot be set. Instead, use Pulse3 as shown in the Gated Measurement example (pulse 1 to pulse 4 would work too, but without the direct Trigger source to Pulse3 internal connection).
Refer to Gated Measurement for an example of how to set up a gated spectrum analyzer measurement.
Warning messages appear when the measurement cannot be performed with the current settings. Messages are displayed in blue for three seconds and the channel is placed in hold (not sweeping).
SA Warning: Image Reject Max and Better are not allowed if RBW > 1MHz and Narrow IF Filter.
SA Warning: Image Reject Max is not allowed if RBW > 1MHz.
SA Warning: Image Reject Better is not allowed if RBW > 2MHz.
SA Warning: Image Reject Max and Better are not allowed below 20 MHz if RBW > 1MHz and Wide IF Filter.
SA Warning: Cannot run Image Reject None LO High at high end of RF frequencies.
SA Warning: Cannot run Image Reject None LO Low at low end of RF frequencies.
SA Warning: Cannot force Narrow IF Filter if RBW > 1MHz.