Write/Read |
About Averaging |
Description |
Specifies the type of averaging to perform: Point or Sweep. |
VB Syntax |
chan.AverageMode = value |
Variable |
(Type) - Description |
|
chan |
A Channel (object) |
|
value |
(Enum as naAverageMode) - Average Type. Choose from: 0 - naPoint Averaging measurements are made on each data point before stepping to the next data point. 1 - naSweep Averaging measurements are made on subsequent sweeps until the required number of averaging sweeps are performed. |
Return Type |
Enum |
Default |
1- naSweep |
Examples |
chan.AverageMode = naSweep 'Write |
|
avgType = chan.AverageMode ' Read |
|
C++ Syntax |
HRESULT get_AverageMode(NAAverageMode * mode); HRESULT put_AverageMode(NAAverageMode mode); |
Interface |
IChannel16 |
Last Modified:
|
8-Jun-2009 |
Not available on 'C' models. |
|
13-Oct-2008 |
MX New topic |