Read-only
About Averaging

AveragingCount Property


Description

Returns the number of sweeps that have been acquired and averaged into the measurements on this channel.  AveragingFactor specifies the number of sweeps to average.  AveragingCount indicates the progress toward that goal.

 VB Syntax

value = chan.AveragingCount

Variable

(Type) - Description

chan

A Channel (object)

value

(Long Integer) - Variable to store the returned count

Return Type

Long Integer

Default

Not Applicable

Example

avgcount = chan.AveragingCount

C++ Syntax

HRESULT get_AveragingCount(long* count)

Interface

IChannel