Write/Read
About Limits

BeginResponse Property


Description

When constructing a limit line, specifies the amplitude value of the start of a limit segment.

 VB Syntax

limtseg.BeginResponse = value

Variable

(Type) - Description

limtseg

A LimitSegment (object)

value

(double) - Amplitude value. No units

Return Type

Double

Default

0

Examples

Set limtseg = meas.LimitTest(1)
limtseg.BeginResponse = 10 'Write

BegResp = limtseg.BeginResponse 'Read

C++ Syntax

HRESULT get_BeginResponse(double *pVal)
HRESULT put_BeginResponse(double newVal)

Interface

ILimitSegment