Write/Read
About Swept IMD

CTBXMODNumCarriers Property


Description

Sets the “N = Total number of carriers” value used in the calculation of the XMOD and CTB parameter. Learn more.

 VB Syntax

imd.CTBXMODNumCarriers = value

Variable

(Type) - Description

imd

A SweptIMD Object

value

(Long Integer) Number of carriers.

Return Type

Long Integer

Default

40

Examples

imd.CTBXMODNumCarriers = 15 'Write

value = imd.CTBXMODNumCarriers 'Read

C++ Syntax

HRESULT get_CTBXMODNumCarriers(double *pVal)
HRESULT put_CTBXMODNumCarriers(double *pVal)

Interface

ISweptIMD