Description |
Sets and returns the name of the Cal Kit to use for unguided cal. |
VB Syntax |
cal.CalKitType (port) = value |
Variable |
(Type) - Description |
cal |
Calibrator (object) |
port |
(Long) Currently unused |
value |
(String) Cal Kit name enclosed in quotes. Use CalKitTypes to read a list of all available Cal Kits in the PNA. |
Return Type |
String |
Default |
Last kit selected |
Examples |
cal.CalKitType(1)= "85052B" |
C++ Syntax |
HRESULT put_CalKitType(long port, BSTR calKit); HRESULT get_CalKitType(long port, BSTR* pCalKit); |
Interface |
ICalibrator10 |
Last Modified:
17-Mar-2010 |
MX New topic |