Write/Read |
About Phase Reference Cals |
Description |
Sets and returns the Cal Kit to be used during the S-parameter portion of a Phase Reference calibration. |
VB Syntax |
phaseRef.CalKitType = value |
Variable |
(Type) - Description |
object |
Any of the following: PhaseReferenceCalibration (object) |
value |
(string) - Calibration Kit type. Case-sensitive. Use GetCompatibleCalKits to return a list of valid Cal Kits. |
Return Type |
String |
Default |
Not Applicable |
Examples |
phaseRef.CalKitType = "85052C" |
value = phaseRef.CalKitType 'Read |
|
C++ Syntax |
HRESULT get_CalKitType(BSTR *calkit) HRESULT put_CalKitType(BSTR calkit) |
Interface |
IPhaseReference2 |
Last Modified:
15-Mar-2013 |
New topic |