Write/Read |
About Cal All |
Description |
For each channel to be calibrated, sets and returns the ports to be calibrated. The port numbers need to be specified only for standard channels. Apps channels have designated input/output/LO ports. Select any of the native PNA ports. |
VB Syntax |
calAll.CalibrationPorts (chan) = ports |
Variable |
(Type) - Description |
|
calAll |
A CalibrateAllChannels (object) |
|
chan |
Channel to be calibrated with a Calibrate All Channels calibration. |
|
port |
(Variant Array) Ports to be calibrated for the specified channel. |
Return Type |
Variant Array |
Default |
Standard channels - ports 1 and 2 Apps channels - the designated input and output ports. |
Examples |
calAll.CalibrationPorts(2) = 0 'Ports to calibrate for channel 2 value = calAll.CalibrationPorts(2) 'returns the ports for channel 2 |
C++ Syntax |
HRESULT get_CalibrationPorts (long channel, Variant ports); HRESULT put_CalibrationPorts (long channel, Variant* ports); |
Interface |
ICalibrateAllChannels |
Last modified:
|
4-Jan-2012 |
New topic |