Write / Read | 
About Frequency Settings | 
Description | 
 Sets and reads the center frequency step size of the analyzer. This command sets the manual step size (only valid when CenterFrequencyStepSizeMode is FALSE. 
  | 
VB Syntax | 
 chan.CenterFrequencyStepSize = value  | 
Variable | 
(Type) - Description | 
| 
 chan  | 
 (object) - A Channel object  | 
| 
 value  | 
 (Double) - Choose a value (in Hz.) below the stop frequency of the analyzer.  | 
Return Type | 
 Double  | 
Default | 
 Default is 40 MHz. When CenterFrequencyStepSizeMode is TRUE, this value is ignored.  | 
Examples | 
 chan.CenterFrequencyStepSize = 1e5 'Write  | 
C++ Syntax | 
 HRESULT get_CenterFrequencyStepSize(Double* pVal); HRESULT put_CenterFrequencyStepSize(Double pVal);  | 
Interface | 
 IChannel25  |