Frequency range is the span of frequencies you specify for making a device measurement.
See other 'Setup Measurements' topics
How to set Frequency RangeYou can also make these settings and more from the Sweep Type dialog. |
|
|
Using front-panel |
Using Menus |
|
|
|
Either of the following pairs of settings determine the frequency range. The last value that you enter determines the X-Axis labels. For example, if you enter the Start and Span values, the X-Axis will show Center and Span labels. Start /Stop - Specifies the beginning and end frequency of the swept measurement range. Center /Span - Specifies the value at the center and frequency range. Either of the following settings determine the number of evenly-spaced data points across the frequency range. Points - Specifies the number of evenly-spaced data points across the frequency range. Learn more about Data Points. Step - Available ONLY in Linear sweep type. Specifies the frequency step size between evenly-spaced data points. Changes to this setting will cause the Points setting to adjust to the closest integer. Any 'remainder' will adjust either the Stop value or Span value depending on which is displayed on the X-Axis label. |
|
Zoom allows you to easily change the start and stop frequencies or start and stop power levels in a power sweep.
Zoom operates on the Active Trace and all traces in the same channel as the active trace, regardless of the window in which they appear.
|
How to Zoom in a measurement window |
Notes
Zoom is NOT available for the following:
|
Measurements with a CW Time sweep or Power sweep are made at a single frequency rather than over a range of frequencies.
How to set CW Frequency |
|
You can also set CW frequency from the Sweep Type dialog box. |
|
|
Using front-panel |
Using Menus |
|
|
|
CW Type a value and the first letter of the suffix (k,m,or g) or use the up and down arrows to select any value within the range of the PNA. |
The resolution for setting frequency is 1 Hz.
The frequency range of the PNA covers several internal frequency bands. The higher the frequency range of the PNA, the larger the number of bands. The source power to your DUT turns off as the stimulus frequency is swept through these band crossings. To learn more, see Power ON and OFF during Sweep and Retrace.
The listed frequencies in the following tables are the stop frequency of the specified band, and the start frequency of the following band.
You can download a PNA Band Structure Readout utility that lists the band crossings for your PNA.
Frequency band crossings are different for the following models:
N5241A and N5242A
|
Band |
Freq (GHz) |
Band |
Freq (GHz) |
Band |
Freq (GHz) |
|
|
0 |
Reserved |
12 |
.396 |
24 |
8.50 |
|
|
1 |
Reserved |
13 |
.500 |
25 |
10.664 |
|
|
2 |
.014 |
14 |
.628 |
26 |
12.00 |
|
|
3 |
.019 |
15 |
1.00 |
27 |
12.80 |
|
|
4 |
.027 |
16 |
1.50 |
28 |
13.51 |
|
|
5 |
.038 |
17 |
2.00 |
29 |
15.40 |
|
|
6 |
.053 |
18 |
3.00 |
30 |
16.00 |
|
|
7 |
.075 |
19 |
3.20 |
31 |
18.00 |
|
|
8 |
.105 |
20 |
4.00 |
32 |
20.00 |
|
|
9 |
.146 |
21 |
5.332 |
33 |
21.328 |
|
|
10 |
.205 |
22 |
6.752 |
34 |
22.50 |
|
|
11 |
.250 |
23 |
8.00 |
35 |
24.00 |
|
|
|
|
|
|
36 |
27.00 |
|
N5244A and N5245A
|
Band |
Freq (GHz) |
Band |
Freq (GHz) |
Band |
Freq (GHz) |
Band |
Freq (GHz) |
|
|
0 |
Reserved |
12 |
.396 |
24 |
8.50 |
36 |
27.008 |
|
|
1 |
Reserved |
13 |
.500 |
25 |
10.664 |
37 |
32.00 |
|
|
2 |
.014 |
14 |
.628 |
26 |
12.00 |
38 |
36.50 |
|
|
3 |
.019 |
15 |
1.00 |
27 |
12.80 |
39 |
40.50 |
|
|
4 |
.027 |
16 |
1.50 |
28 |
13.51 |
40 |
42.656 |
|
|
5 |
.038 |
17 |
2.00 |
29 |
15.40 |
41 |
43.50 |
|
|
6 |
.053 |
18 |
3.00 |
30 |
16.00 |
42 |
46.20 |
|
|
7 |
.075 |
19 |
3.20 |
31 |
19.00 |
43 |
48.00 |
|
|
8 |
.105 |
20 |
4.00 |
32 |
20.00 |
44 |
50.20 |
|
|
9 |
.146 |
21 |
5.332 |
33 |
21.328 |
|
|
|
|
10 |
.205 |
22 |
6.752 |
34 |
24.00 |
|
|
|
|
11 |
.250 |
23 |
8.00 |
35 |
26.50 |
|
|
|
N5247A
|
Band |
Freq (GHz) |
Band |
Freq (GHz) |
Band |
Freq (GHz) |
|
0 |
Reserved |
12 |
6.75 |
24 |
32.00 |
|
1 |
Reserved |
13 |
8.00 |
25 |
40.00 |
|
2 |
.053 |
14 |
10.70 |
26 |
40.50 |
|
3 |
.175 |
15 |
13.50 |
27 |
42.70 |
|
4 |
.250 |
16 |
15.40 |
28 |
46.20 |
|
5 |
.500 |
17 |
16.00 |
29 |
48.00 |
|
6 |
1.000 |
18 |
19.00 |
30 |
50.00 |
|
7 |
2.000 |
19 |
20.00 |
31 |
54.00 |
|
8 |
3.000 |
20 |
21.30 |
32 |
60.00 |
|
9 |
3.200 |
21 |
24.00 |
33 |
64.00 |
|
10 |
4.000 |
22 |
26.50 |
34 |
67.00 |
|
11 |
5.330 |
23 |
27.00 |
35 |
70.00 |
N5221A and N5222A
|
Band |
Freq (GHz) |
Band |
Freq (GHz) |
|
0 |
Reserved |
12 |
6.752 |
|
1 |
.010 |
13 |
8.0 |
|
2 |
.053 |
14 |
10.664 |
|
3 |
.175 |
15 |
13.51 |
|
4 |
.250 |
16 |
15.40 |
|
5 |
.500 |
17 |
16.0 |
|
6 |
1.0 |
18 |
20.0 |
|
7 |
2.0 |
19 |
21.328 |
|
8 |
3.0 |
20 |
24.0 |
|
9 |
3.2 |
21 |
27.0 |
|
10 |
4.0 |
22 |
|
|
11 |
5.332 |
23 |
|
N5224A and N5225A
|
Band |
Freq (GHz) |
Band |
Freq (GHz) |
Band |
Freq (GHz) |
|
0 |
Reserved |
12 |
6.752 |
24 |
32.00 |
|
1 |
Reserved |
13 |
8.00 |
25 |
40.50 |
|
2 |
.053 |
14 |
10.664 |
26 |
42.656 |
|
3 |
.175 |
15 |
13.51 |
27 |
43.50 |
|
4 |
.250 |
16 |
15.40 |
28 |
46.20 |
|
5 |
.500 |
17 |
16.00 |
29 |
48.00 |
|
6 |
1.000 |
18 |
19.00 |
30 |
50.20 |
|
7 |
2.000 |
19 |
20.00 |
|
|
|
8 |
3.000 |
20 |
21.328 |
|
|
|
9 |
3.200 |
21 |
24.00 |
|
|
|
10 |
4.000 |
22 |
26.50 |
|
|
|
11 |
5.332 |
23 |
27.008 |
|
|
N5227A
|
Band |
Freq (GHz) |
Band |
Freq (GHz) |
Band |
Freq (GHz) |
|
0 |
Reserved |
12 |
6.752 |
24 |
32.00 |
|
1 |
.010 |
13 |
8.00 |
25 |
40.00 |
|
2 |
.053 |
14 |
10.664 |
26 |
40.50 |
|
3 |
.175 |
15 |
13.51 |
27 |
42.656 |
|
4 |
.250 |
16 |
15.40 |
28 |
46.20 |
|
5 |
.500 |
17 |
16.00 |
29 |
48.00 |
|
6 |
1.000 |
18 |
19.00 |
30 |
50.00 |
|
7 |
2.000 |
19 |
20.00 |
31 |
54.00 |
|
8 |
3.000 |
20 |
21.328 |
32 |
60.00 |
|
9 |
3.200 |
21 |
24.00 |
33 |
64.00 |
|
10 |
4.000 |
22 |
26.50 |
34 |
67.00 |
|
11 |
5.332 |
23 |
27.008 |
35 |
70.00 |
N5231A, N5232A, N5239A
|
Band |
Freq (GHz) |
Band |
Freq (GHz) |
|
0 |
Reserved |
10 |
5.33 |
|
1 |
.0003 |
11 |
6.75 |
|
2 |
.000425 |
12 |
8.00 |
|
3 |
.0012 |
13 |
10.07 |
|
4 |
.0075 |
14 |
13.50 |
|
5 |
.250 |
15 |
16.00 |
|
6 |
.500 |
16 |
16.70 |
|
7 |
1.00 |
17 |
20.01 |
|
8 |
3.00 |
|
|
|
9 |
4.00 |
|
|
|
Band |
Freq (GHz) |
Band |
Freq (GHz) |
Band |
Freq (GHz) |
|
0 |
|
11 |
10.66 |
21 |
30.80 |
|
1 |
.010 |
12 |
13.51 |
22 |
31.50 |
|
2 |
.250 |
13 |
15.40 |
23 |
32.00 |
|
3 |
.500 |
14 |
16.00 |
24 |
40.00 |
|
4 |
1.00 |
15 |
20.00 |
25 |
40.56 |
|
5 |
2.00 |
16 |
20.26 |
26 |
42.00 |
|
6 |
3.00 |
17 |
21.33 |
27 |
48.00 |
|
7 |
4.00 |
18 |
24.00 |
28 |
50.00 |
|
8 |
5.332 |
19 |
26.00 |
|
|
|
9 |
6.752 |
20 |
27.01 |
|
|
|
10 |
8.00 |
|
|
|
|