Write/Read
 

CharFileName Property


Description

Specifies the mixer characterization (.S2P) file and immediately loads the file. Also specify the use of a characterization file with LoadCharFromFile Property

 VB Syntax

VMC.CharFileName = value

Variable

(Type) - Description

VMC

VMCType (object)

value

(String)  Full path, file name, and extension of the mixer characterization file.

Return Type

Not Applicable

Default

Not Applicable

Examples

VMC.CharFileName = "c:\users\public\network analyzer\documents/default.S2P"

C++ Syntax

HRESULT put_CharFileName(BSTR filename);

HRESULT get_CharFileName(BSTR *filename);

Interface

VMCType