Description
Contains the methods and properties to perform a Vector Measurement Calibration for the Frequency Converter Application (option 083).
See an example which creates and calibrates a VMC measurement.
You can also do the following:
Set app = CreateObject("AgilentPNA835x.Application") Set CalMgr = app.GetCalManager Set guidedCal = CalMgr.CreateCustomCalEx(1) Set VMC = guidedCal.CustomCalConfiguration VMC.ConnectorType(1) = "APC 3.5 male" |
Methods |
Interface |
Description |
---|---|---|
IVMCType |
Acquire the measurement data for the specified step in the calibration process. |
|
IVMCType |
Generates the error terms for the calibration. |
|
IVMCType |
Returns the number of steps required to complete the calibration. |
|
IVMCType |
Returns the description of the specified step in the calibration process. |
|
IVMCType |
Begins a calibration. |
|
Properties |
|
Description |
IVMCType |
Sets ECAL module automatic orientation ON or OFF. |
|
IVMCType |
Sets and returns a calibration kit type for calibration. |
|
IVMCType |
Sets and returns whether to perform a mixer characterization ONLY or full 2-port calibration. |
|
IVMCType |
Specifies the .S2P mixer characterization file name. |
|
IVMCType2 |
Specifies the direction in which to characterize the calibration mixer. |
|
IVMCType |
Returns a list of cal kits that are compatible with the connector type for the specified port. |
|
IVMCType |
Sets or queries the connector type for the specified port. |
|
IVMCType |
Superseded with CalKitType Specify ECAL or Mechanical calibration for the mixer characterization portion of a VMC calibration. |
|
IVMCType |
Superseded with CalKitType Specify ECAL or Mechanical calibration for the 2-port calibration portion of a VMC calibration. |
|
IVMCType |
Superseded with CalKitType Specifies the characterization data within an ECal module to be used for the calibration. |
|
IVMCType |
For Mixer Characterization ONLY - Specifies which port of the ECal module is connected to which port of the PNA |
|
IVMCType |
For full 2-port VMC cal - Specifies which port of the ECal module is connected to which port of the PNA |
|
IVMCType4 |
Perform LO Power Cal |
|
IVMCType |
Specifies and loads a mixer characterization (S2P) file. |
|
IVMCType3 |
Specifies the S2P filename to embed or de-embed on the input or output of your mixer measurement. |
|
IVMCType3 |
Embed (add) or de-embed (remove) circuit network effects on the input and output of your mixer measurement. |
|
IVMCType |
Superseded - Replaced by SetIsolationPaths and GetIsolationPaths Sets and returns whether Isolation portion of the calibration will be performed or not. |
|
IVMCType |
Superseded - Replaced by PathThruMethod Property Sets and returns the method for performing the thru portion of the calibration. |
|
IVMCType |
Returns a list of connector types for which there are calibration kits. |
Interface |
Introduced with PNA Rev: |
IVMCType |
3.5 |
IVMCType2 |
3.53 |
IVMCType3 |
6.0 |
IVMCType4 |
9.1 |