Write/Read
About Citifiles

CitiContents Property - Superseded


Description

This command is replaced with SaveData Method

Specifies the contents of subsequent citifile saves using app.SaveCitiDataData or app.SaveCitiFormattedData

 VB Syntax

pref.CitiContents = value

Variable

(Type) - Description

pref

A Preferences (object)

value

(string) - Contents that will be saved with subsequent save commands. Choose from:

"Single" - Single trace

"Displayed" - All displayed traces

"Auto" - All displayed traces

Return Type

String

Default

"Auto"

Examples

pref.CitiContents = "Single" 'Write

content = pref.CitiContents 'Read

C++ Syntax

HRESULT get_CitiContents(BSTR *Contents)
HRESULT put_CitiContents(BSTR Contents)

Interface

IPreferences